New Features
XP Universal Driver 4.40 has the
following new features:
-
The XP Universal driver package
is has been localized to support the English, French, German, Spanish, Italian,
Japanese, Simplified Chinese and Traditional Chinese.
-
To keep the size of the Elo XP
Universal driver default download package to a minimum, the XP Universal Driver
package is provided as two separate packages:
- Driver package
- Users Guide
-
The XP Universal Users Guide is
also localized to support the English, French, German, Spanish, Italian,
Japanese, Simplified Chinese and Traditional Chinese. The English Users Guide
is included in the default download package. Language specific users guides can
be downloaded from http://www.elotouch.com/support/dnld.asp
-
Default calibration
configuration values are saved in the Elo software registry key or in a file
that can be modified to support user specific calibration values.
-
Surface Capacitive calibration
has been modified to automatically timeout after 30 seconds if there is no user
interaction. Previous versions made five attempts before switching to the next
monitor or exiting.
-
The transparency of the right
click on hold timeout icon is configured by a registry value entry. Please see
Appendix A for details on how to use this feature.
-
The initial delay before the
right click on hold time out icon appears is configured by a registry value
entry. Please see Appendix A for details on how to
use this feature.
-
If the system does not have a
keyboard and mouse connected to it, the disable touch feature cannot be used
from the task bar or control panel.
-
For Infrared touchmonitors,
special support has been added to detect and report blocked beams. The Advanced
page for the touchmonitor in the Control Panel is used to configure this
feature.
-
A special hardware beep
configuration feature for Infrared touchmonitors that include this special
hardware feature has been added. The Advanced page for the touchmonitor in the
Control Panel is used to configure this feature.
XPU 4.4 can be preinstalled on a
system that has no support for a mouse or HID devices, however, this requires
the user to insert the Windows system disk during the installation.
Bug fixed in this version:
-
Intermittent loss of touch and
activation of and the "Disable Touch" feature in the Elo control panel
-
Windows Server 2003 would hang
during the boot process because the Elo Service Application failed to load.
-
The EloGetTouch API function
would not return touch data within a "no touch" rectangle. It now returns touch
data irrespective of the touch rectangles defined on the screen.
-
The EloGetTouch API function
reports incorrect coordinates in 'Drag' mode.
-
The installation application
sometimes causes a system message pop-up dialog box that prompts users to
select the file location when installing a Serial only package.
-
The tool tray menu sometimes
hides the taskbar. It now appears above the taskbar and is larger to permit
easier option selection.
-
The touch mode sometimes changes
to Mouse emulation mode after the video alignment application exited with a
timeout.